Operator system interaction

The operating stations used on process control systems allow operators to monitor and control process engineering plants conveniently and reliably. They can be used to monitor the current state of the plant as well as process values and alarms. They also provide support to operators for manual controller of processes, such as starting and stopping motors. The system status, trends and historical data are represented graphically and the ability to display alarms contributes significantly to error correction. The report server generates detailed reports that include process data, alarms, trends and all events.

APROL Engineering desktop

Workstation functionality

Tooltips provide detailed information

Menu items are provided with meaningful tooltips to display detailed information about the respective programs.

Touch screen virtual keyboard

A virtual keyboard can be used to implement touch screen solutions or provide help if the physical keyboard fails.

Access via web browser

Taking into account the required access rights, the entire operator interface can be started from a Microsoft Windows 11 computer via VNC (Virtual Network Computing) using a VNC viewer.

Web access without configuration effort

Users can carry out operation and monitoring tasks, complete historical evaluations of alarms, events or trend curves, call up logs and start various diagnostic tools for network equipment or hardware and software components without additional configuration effort and without functional restrictions.

Multiscreening

 Support for 1, 2, 3, 4 screens

Multiscreening with a keyboard/mouse makes it possible to connect several screens to one operator station. Depending on the graphics card, 1, 2, 3, 4 or even 8 screens can be used with a single operator station.

Flexible assignment of images

The flexible assignment of images makes it possible to display a different process graphic, trend diagram or alarm monitor on each of these screens and to operate them using a mouse and keyboard.

Multiscreening

Operation and monitoring

DisplayCenter for interaction

DisplayCenter acts as the central application for process control. In the process graphic, the operator can see all current process states and intervene interactively depending on the defined permissions.

Personalized user environment

Depending on which operators are logged in, different configurations for the appearance (such as menu bar, toolbar and graphic tree) can be stored. This means that only the visualization elements relevant to each operator are displayed.

Process graphic history

The most recently used process graphics can be called up quickly using the forward and back buttons (similar to a web browser). It is also possible to select the last 11 activated process graphics directly via menu entries.

Operator interventions are fully logged

All operator interventions are coordinated via the authorization system and securely logged via the integrated AuditTrail (in accordance with the requirements of 21 CFR Part 11 and GAMP5).

The look and feel is freely configurable

In addition to the functionality, the look and feel are adapted according to company-specific operating philosophies. This enables user-friendly migration of old process control systems without compromising plant availability by retaining the familiar user environment.

Button text

DisplayCenter

Operation and monitoring

Graphic tree for navigation

The graphic tree presents all configured process graphics with their corresponding names and descriptions. These images can be selected directly from here.

Process graphic text search

The integrated full-text search in the graphic tree also makes it possible to search for a specific process graphic or device.

Favorites for important images

Each operator can save process graphics as favorites in the graphic tree during runtime, similar to a web browser. This enables quick access to the most frequently used process graphics.

Button text

Graphic tree / Favorites

Process graphics with Tooltips

In Engineering, Tooltips can be stored for each device. They are shown to the operator when moving the mouse over the corresponding object. The Tooltips can even contain images and process values.

Process graphics with scalable vector graphics

A variety of image formats, such as bmp, jpg, png and svg (scalable vector graphics), can be embedded as a background for process graphics.

Integrated calls from the process graphic

Web page calls (system messages, AuditTrail, logs, system and project documentation) and the playback of video sequences or even remote control of entire computers can be embedded directly in the process graphic.

Process graphics

VncViewer functionality

VncViewer as a visualization element

DisplayCenter provides the AprolVncViewer and VncViewer visualization elements for embedding in a process graphic.

AprolVncViewer as an embedded app

The AprolVncViewer can be integrated into a process graphic as an embedded app.

APROL VncViewer

VncViewer visualization element

HMI applications can be embedded in a process graphic using the VncViewer visualization element.

Authentication is supported

The VncViewer visualization element supports all standard functions such as locking and verification as well as extended authentication during interaction in the HMI application (two-man rule) and logging in the AuditTrail.

Frame indicates existing permission

When a VNC view is activated, it is displayed in read-only mode in a thin black frame. This frame is colored in the selection color (yellow) when the operator clicks once with the mouse in this VNC view and receives permission to perform interactions in the VNC view (read/write mode).

VncViewer visualization elements in a process graphic

Online parameter management

Easy handling of online parameters

The faceplate view (measuring points / online parameters) and control module view (online parameter groups) are available to clearly display and easily edit online parameters.

Commissioning

The application software is simplified by a list display. This not only makes it easier to enter missing parameters (runtimes, delays, etc.), but also allows the "Inhibit" flag of several control modules to be enabled at the same time.

Operating dialog boxes allows comparison

Dialog boxes allow all parameters for a measurement point to be displayed at the same time as well as comparison of several measurement points. Existing online parameters can also be transferred to other measurement points using these dialog boxes. When importing the online parameters into the project created in B&R's CaeManager engineering tool, a new version is automatically created with the version comment "Online parameters imported".

Online parameter management structure

ParameterCenter for batch production

For discontinuous batch processes

Controller of discontinuous batch processes via ParameterCenter

Configuration using templates

Definition of equipment and parameter set templates (based on the S88 standard) in the engineering system.

Parameter set defines product

Parameter sets represent products in the system (e.g. parameter set 1 for manufacturing product A and parameter set 2 for manufacturing product B).

Upload/Download functionality for product handling

Parameter sets can be changed by the operator or automatically using a preselection program (e.g. changeover of production from product A to product B) Management with MySQL

Parameter set can be changed flexibly

Parameter sets are created and changed in the engineering system and can also be implemented by the operator at runtime.

Managing with MySQL

Parameter sets are managed in a MySQL database. An open interface allows data to be imported and exported to a production planning system.

Import/Export interfaces

The ParameterManagement tool allows data to be imported/exported to/from the parameter set database of the runtime server.

All actions are logged by the AuditTrail

The integrated AuditTrail (21 CFR Part 11, GAMP4) logs all operator actions in the parameter and makes this important information (who, what, when, where) available in web form.

System structure - Parameter set template

System structure - Parameter set

Security login

Access/Operator rights

The access rights in the process-based HMI application are defined via the operator rights. These rights can be freely defined in the project.

Convenient user management with the OperatorManager

Clear management of operators and groups in one user interface. The roles of the operators are determined by defining groups. In the OperatorManager, users are assigned to one or more groups. The assigned groups determine the action that can be carried out by the specific operator in the process control system.

Any number of operators and groups

As many operators and groups as needed can be created in the system.

Uniform representation

Uniform representation for access/operator administration in the engineering and runtime environments makes managing user rights fast and intuitive.

Export/Import interface

Interface for exporting/importing operator rights in secure binary format simplifies configuration.

The block output contains a defined right

When creating image macros in libraries, they are configured in such a way that they can be used to directly intervene in the process. In the image macro, this object is then a block output. An operator right is assigned to this block output.

Access rights

Operator rights are inherited through libraries in the project. In addition, there are the rights of the graphic blocks that may have been overwritten in the hyper macros, as well as the rights defined in the project.

OperatorManager application - Operators/groups

Security login

Access/Operator rights

The access rights in the process-based HMI application are defined via the operator rights. These rights can be freely defined in the project.

Convenient user management with the OperatorManager

Clear management of operators and groups in one user interface. The roles of the operators are determined by defining groups. In the OperatorManager, users are assigned to one or more groups. The assigned groups determine the action that can be carried out by the specific operator in the process control system.

Any number of operators and groups

As many operators and groups as needed can be created in the system.

Uniform representation

Uniform representation for access/operator administration in the engineering and runtime environments makes managing user rights fast and intuitive.

Export/Import interface

Interface for exporting/importing operator rights in secure binary format simplifies configuration.

The block output contains a defined right

When creating image macros in libraries, they are configured in such a way that they can be used to directly intervene in the process. In the image macro, this object is then a block output. An operator right is assigned to this block output.

Access rights

Operator rights are inherited through libraries in the project. In addition, there are the rights of the graphic blocks that may have been overwritten in the hyper macros, as well as the rights defined in the project.

Application rights

Defining application rights determines which runtime system applications are allowed to be started and which actions are permitted within these applications.

Various login options

Logging in is done using the keypad, chip card reader or transponder reader and password on the operator station. The configured rights are automatically assigned by the login server. It is also possible to integrate a company's existing chip cards.

Personalized user environment

Depending on the operator currently logged in, process graphics, units and alarms are displayed on the user interface.

Logic-dependent login option

An operator logging in can be permitted or prevented depending on arbitrarily defined logic, e.g. depending on the system status.

Automatic logout

If the logged-in operator does not make any entries during a defined period of inactivity, they can be automatically logged out of the login server. The operator idle time thus prevents another user from working on the workstation with these login credentials.

AuditTrail monitors all login/logout activities

All operator activities (login/logout) are seamlessly recorded in a tamper-proof database, the so-called AuditTrail.

OperatorManager application - Process graphics display rights

AuditTrail

Recording and monitoring of all operator activities

All operator activities are seamlessly recorded in a tamper-proof database, the so-called AuditTrail.

Supports fulfillment of requirements, e.g. according to 21 CFR Part 11 and EU 178/2002

Complete traceability of operator activities supports, for example, the fulfillment of pharmaceutical industry requirements through GAMP (Good Automated Manufacturing Practice), 21 CFR Part 11 of the American Food and Drug Administration (FDA) or Regulation EU 178/2002, which applies to the food and beverage industry. Reliable recording of operator actions in an AuditTrail enables the system operator to have paperless, seamless traceability of all operator activities that are subject to document control.

Complete overview of all operator activities performed

Depending on the operator activities, detailed information such as security login (operator logs in or out), interactive process execution, external process execution (web interface), process visualization (image opened, faceplate operated), system control actions (start, end, initialization of various applications), controller management (start, end, service/diagnostics mode), alarm suppression (lock, release), parameter history (download of parameter sets, modification of parameters) and the modification of protocol data (entry of replacement values) are seamlessly recorded in a database.

AuditTrail database contains all detailed information

All essential data is recorded as a complete description of the action. This can include the time and date of changes, operator login, device, project ID, APROL system, server and operator terminal, controller action, old and new values, alarm and alarm group, event/function, comment/reason for change, image description and graphic block, web access and changed process variables, parameter set, ParameterCenter mode, reason for change, category and name of changed protocol data.

Clear record of the action in terms of when? What?, Who?, Where?

Each entry in the AuditTrail has the following detailed information:

Date and time = When
Action performed = What (incl. old/new value)
Name of the operator = Who
Location of the current comprehensive AuditTrail with filter functions can be queried very conveniently = Where

Comprehensive AuditTrail with filter functions can be queried very conveniently

Filters can be used to create the desired view of the AuditTrail data. The data can be easily exported as an HTML file. Stored data cannot be changed or deleted and is therefore considered largely tamper-proof, which fulfills a central FDA requirement according to 21 CFR Part 11.

System functionality – AuditTrail runs without prior configuration

AuditTrail is always started automatically, so no configuration is necessary or misconfiguration is possible. This means that the AuditTrail data is always available.

Access rights regulate access to AuditTrail

Authorization to access the data recorded by the AuditTrail is defined in the engineering environment via the APROL authorization system (2-component authorization consisting of user login + password).

Data can be further processed with Office applications

All data can be imported into applications (HTML, CSV format), printed out or saved as a PDF document without additional programs (in MS Office, Open Office, etc.).

AuditTrail report

Language switching

Publication in German and English

APROL releases are generally provided in German (de) and English (en). This also applies to the APROL system documentation.

The TranslationManager enables translations

With the integrated translation tool TranslationManager, users can easily create missing translations in the APROL system software modules (e.g. DisplayCenter, etc.) and in the APROL project themselves.

Different degrees of translation

Other languages listed below are available with varying degrees of translation. The APROL system software modules for the engineering environment are not available for the most part, since a translation is mainly only required for operating and monitoring (operator station).

Partially implemented languages or prepared environments

Partially implemented languages or prepared environments:
• Chinese (zh_CN) • Traditional Chinese (zh_TW) • Danish (da) • Finnish (fi) • French (fr) • Italian (it) • Japanese (ja) • Korean (ko_KR) • Lithuanian (lt) • Dutch (nl) • Norwegian (no) • Polish (pl) • Portuguese (pt) • Romanian (ro) • Russian (ru) • Swedish (sv) • Slovakian (sk) • Spanish (es) • Czech (cs) • Turkish (tr) • Hungarian (hu)

Any alphabets and character sets

All alphabets and character sets used worldwide can be displayed in APROL thanks to its UNICODE capability (UTF-8). To use multiple languages in parallel, e.g. in the HMI application, the corresponding information and texts can be stored separately for each language in the engineering environment.

Language-dependent texts in the HMI application

APROL supports language switching for the HMI applications in all supported target languages. The texts in the process graphics are displayed at runtime in the set target language.

Localization of the alarm texts

The alarm texts can be translated into another language. During runtime, the alarm texts can be displayed on the operator station in the DisplayCenter and in the alarm report in the translated language.

Compendium contains all HMI texts

The texts used in the libraries on the input pins, faceplates, static tooltips, etc. are summarized in a compendium so double translations are not required.

TranslationManager for translation in list form

The TranslationManager provides convenient translation of HMI texts in list form. Efficient translation performance is ensured by specifying a status when displaying original and translation texts as well as support through translation suggestions based on a loadable compendium.

The translation texts are downloaded automatically

The host computers receive the translation texts automatically via the usual download mechanism.

Language switching - System structure

Veuillez sélectionner un pays et une langue

B&R Logo